AXIS#.UNIT.PROTARY

Description

AXIS#.UNIT.PROTARY sets the position units when the motor type (AXIS#.MOTOR.TYPE ) is rotary.

Value

Units

0

counts

1

rad

2

degs

3

Custom Units

4

counts 16-bit

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 4

Default Value

4

Data Type

Integer

See Also

AXIS#.PL.FB, AXIS#.PL.CMD, AXIS#.MOTOR.TYPE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.UNIT.PROTARY

5010h

05h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6605

1

6605 (0x19cd)

AXIS1.UNIT.PROTARY

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.UNIT.PROTARY

6605

Unsigned8

Read/Write

-